AnsweredAssumed Answered

Calibration mode One-path 2-Port Cal

Question asked by blesia on Mar 7, 2007
Latest reply on Mar 12, 2007 by daveb
Hello !

I use an VNA HP8753C for a fews weeks, and I haven't problem with calibration S11 1-port or full-two-ports, but I don't know realize a calibration with 1-path 2-port Cal, the operating manual is not clear. What is the "test port" ? And "the return cable to analyzer" ? Also, when I disconnect the S-parameter test set, I have the error message "Caution: no if found: check R input level"

Can I really realize a calibration without this S-parameter test set, as it write in the operating manual ?  

Outcomes