AnsweredAssumed Answered

Programmatic selection of eCal characterization on 8363/4

Question asked by neilr on Sep 7, 2007
Latest reply on Sep 11, 2007 by neilr
Hopefully this should be an easy one for someone familiar with the 8363/4 eCal. How do you programmatically (using SCPI) select the active characterization when performing an eCal on an 8363/4 ?
I see that a list of characterizations can be returned using SENS:CORR:CKIT:ECAL:CLISt? but can't find an option to select the characterization in the way that you do manually when running through the Cal Wizard.

Any ideas ?

Thanks
Neil Richardson
Astrium
Test & Software Group
UK  

Outcomes