AnsweredAssumed Answered

Problems with Intuilink Data Capture 3.6

Question asked by Mr.H on Sep 11, 2009
Latest reply on Sep 18, 2009 by dnt
I'm having issues getting Intuilink Data capture to work

Hardware I have:

DSO7104A
PC running Windows XP SP2


Software I have:

Agilent IO Libraries Suite 15.5
Intuilink Data Capture 3.6


The scope shows up fine in the Agilent Connection Expert and I can communicate with it with the interactive I/O. However, when I launch Intuilink Data Capture, I'm shown the message "Agilent IntuiLink Data Capture requires the Agilent I/O Libraries for connections to the instruments. Connections to the instruments via GPIB, LAN, USB etc needs to be configured first in the I/O Libraries. For USB connections, Agilent I/O Libraries version M.01.00 or later is required."

If I press OK in that dialogue box and then choose Agilent 7000 series from the "instrument" menu, the only option seems to be GPIB; if I then click on the "find instrument" button, the only option then is COM1.

What am I doing wrong?  

Outcomes