AnsweredAssumed Answered

Measuring peak-to-peak voltage of 86100C using Labview

Question asked by billheadley on Aug 12, 2009
Latest reply on Aug 20, 2009 by dnt
Hello,

I am using Labview 8.5 to control my DCA86100C using theIVIAgilentInfiniuumDCA IVI-COM library.  I was wondering if it is possible to obtain the peak-to-peak voltage value that is measured by the DCA when it is in scope mode from one of the library controls.  Or will I have to read the waveform first and then do the calculation within Labview?

Cheers,
Bill  

Outcomes