AnsweredAssumed Answered

Configuring the Lightwave Component Analyzer

Question asked by mkelly Employee on Feb 13, 2007
Latest reply on Feb 13, 2007 by olfu
A user has an 8510-8514B with a Lightwave 83420A test set (opt 012, 100, 210, H03) which is used to evaluate electro-optical components.

Can the Lightwave 83420A test set be used with the new PNA-L series, like in the N4373A?  

Outcomes