Hi Guys
I have written a matlab code to obtain the values of a waveform from oscilloscope. I have set the encoding to be binary. But the obtained waveform values is
#41000ñññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññðððððððððððððððððððððððððððððððððððððððððððððððððððððððððððððððððððððññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòò
The preamble information is
1;8;BINARY;RI;LSB;"Ch1, DC coupling, 1.000mV/div, 625.0ns/div, 25000000 points, Sample mode";1000;Y;"s";250.0000E-15;0.0000;12500000;"V";40.0000E-6;0.0000;0.0000;1
I think I need to process the obtained values to get the actual voltage values. Can someone please guide me on how to process the above obtained values in order to find the actual voltage values transferred. Can someone please explain what would be the next step? Thanks
I have written a matlab code to obtain the values of a waveform from oscilloscope. I have set the encoding to be binary. But the obtained waveform values is
#41000ñññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññðððððððððððððððððððððððððððððððððððððððððððððððððððððððððððððððððððððññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññññòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòòò
The preamble information is
1;8;BINARY;RI;LSB;"Ch1, DC coupling, 1.000mV/div, 625.0ns/div, 25000000 points, Sample mode";1000;Y;"s";250.0000E-15;0.0000;12500000;"V";40.0000E-6;0.0000;0.0000;1
I think I need to process the obtained values to get the actual voltage values. Can someone please guide me on how to process the above obtained values in order to find the actual voltage values transferred. Can someone please explain what would be the next step? Thanks
Attached is the code I wrote do transfer the waveform data.
It's in visual basic, but you should be able to translate it easily.
For converting the bytes to a floating point number, there should be a command in whatever language you use to do this.
Note: the code will not compile or anything...it should just be used as a reference on what to do.
Alternatively, you could use something besides binary format...it'll be MUUUUCH slower, but, easier to process.