Hello,
i want to capture some hardcopies via intuilink toolbar into my excelsheet. Connection to MSO6034A is done via USB. The agilent connection expert is showing the scope beneath the USB0 and i can communicate with the MSO.
When starting excel and trying to connect to the MSO a small window pops up saying "searching busses" or something like that. After the window has disappeared, another window "find instrument" comes up, where only a COM1 interface is listed. An USB interface is nowhere to be seen. It seems to me, that i have to add the USB to the busses to be searched, but i have no idea where to do this.
Any ideas?
Thanks.
i want to capture some hardcopies via intuilink toolbar into my excelsheet. Connection to MSO6034A is done via USB. The agilent connection expert is showing the scope beneath the USB0 and i can communicate with the MSO.
When starting excel and trying to connect to the MSO a small window pops up saying "searching busses" or something like that. After the window has disappeared, another window "find instrument" comes up, where only a COM1 interface is listed. An USB interface is nowhere to be seen. It seems to me, that i have to add the USB to the busses to be searched, but i have no idea where to do this.
Any ideas?
Thanks.
can communicate to the 6000 using the IO libraries VISA Assistant.
Second, try connecting to the scope using Intuilink Data Capture.
IDC is a little more verbose on connection issues.
Also, if you haven't downloaded the Intuilink tools in a while try
the current version at www.agilent.com/find/intuilink or
http://www.home.agilent.com/agilent/edi ... &id=670621