So exactly how are you suppose to do this with the command set for the scope? I am using the DSO-8 series 10GHz scope connected to a private LAN with a PC. I have read the programming manual and cannot find anything obvious as to how this can be done. If you can answer this or provide some programming examples, that would be great. I have to imagine this is a very common request, no?
as well, I have these questions below:
1. Is it possible to make the c:\ drive on the scope shareable on the network such that a PC can simply copy files from it? I'm assuming it should be since the scope seems to run Win XP.
dave mc
as well, I have these questions below:
1. Is it possible to make the c:\ drive on the scope shareable on the network such that a PC can simply copy files from it? I'm assuming it should be since the scope seems to run Win XP.
dave mc
format. Save the returned binblock to a file with the appropriate
extension for the format selected.
The DSO80000 scope is a Windows platform and is subject to the same
constraints as any other Windows platform. If you are operating a Windows Domain the scope must be set up as a member of the Domain.
Likewise with a Workgroup.