How I can use the oscilloscope for measuring real time signals.
when I load VSA , a message " simulated hardware" is displayed on graph display. I unchecked the simulated H/W in utilities>>hardware menue,but problem is unrersoleved.
regard fahim :?:
when I load VSA , a message " simulated hardware" is displayed on graph display. I unchecked the simulated H/W in utilities>>hardware menue,but problem is unrersoleved.
regard fahim :?:
Insure that you are running the latest versions of the Infiniium SW and 89601A SW. Insure that you have option 300 (hardware connectivity). Also insure that the 89601A SW is not running on a "demo" licence, which does not support HW. The 15 day trial licence does support HW. If all this checks out, but still no connectivity to the scope HW, then run Agilent I/O library connection expert and see if there is I/O connectivity to the scope. If no connectivity then see view
In the specific case of the DSO 80000B as it is no longer a current shipping product, it may not be supported by the latest shipping version of 89601A SW, as of 10/9/08 that would be version 9.0. In this case I would recommend downloading version 8.0 at http://www.home.agilent.com/agilent/edi ... id=1303376