Hi,
We are having test board in EE dept and Logic analyzer in CE dept.
We have to test wave forms. How can this be done?
1. We cannot connect such a long probe from one dept to another.
Is there any other way to do it.
We are having test board in EE dept and Logic analyzer in CE dept.
We have to test wave forms. How can this be done?
1. We cannot connect such a long probe from one dept to another.
Is there any other way to do it.
The logic analyzer must be close enough to the system under test to connect the probes to the logic analyzer. Most LA cables are about 3 ft long.
Depending on the model of logic analyzer you are using, it could be possible to use remote desktop or control the LA from a PC in another location over the LAN.
Best Regards,
Jennie