The new 82357B USB to GPIB adapter is out. It's very nice and USB 2.0 but you need a secret driver to get it to work with the Agilent I/O libraries 14.2. This is the latest version of the I/O libraries and makes no mention of the extra driver you need. The 82357B web site also makes no mention of this driver, nor does the 82357B manual. It is available at the following link:
So to get an 82357B (the 'A's are now obsolete) to work you need to install the I/O libraries version 14.2 and then the 82357B driver. Do this before you plug in the 82357B and it works great.
ftp://ftp.agilent.com/pub/callpub2/lightwav/82357B/
So to get an 82357B (the 'A's are now obsolete) to work you need to install the I/O libraries version 14.2 and then the 82357B driver. Do this before you plug in the 82357B and it works great.