Does MSO6054A allow state mode?
Timing mode works great, but uses up the memory too fast.
I want to use rising edge of data 0 as a clock for d1-d12.
I can't see how to do it with GPIB commands.
Can someone drop a quick code snippet for help?
Timing mode works great, but uses up the memory too fast.
I want to use rising edge of data 0 as a clock for d1-d12.
I can't see how to do it with GPIB commands.
Can someone drop a quick code snippet for help?
Look under the Trigger commands if you have one of the analysis options.
E.g.:
:trig:spi:source:clock d0