When I read release notes for the latest software release V5.2 - I thought cool - finally a waveform tracking cursors. However I was soon disappointed when I found out that I actually need a MST licence to make them work. Given this I think your release notes are misleading.
Regards
tomasz.
Regards
tomasz.
Sometimes even stuff that was initially advertised as being standard (RS232 trigger).
Most of the options are about 10% the cost of the scope, which seems a bit ridiculous - I'm sure they'd sell a lot more if they were cheaper.
Let's hope Tek start offering stuff like this for free to provide some competition & encourage Agilent to match it.