Hi. I need help with measure the delay between two waveforms using the rising edges. I can show it on display but I don´t know how to transport the date to the program in VEE. I use the OSC DSO3062. I measure two sinus signal and i need meas the delay between two waveforms. How to enable digital filter in VEE on DSO3062? THX for help.
I meas with:
Automatic Measurements - Time Measurement Menu 3 - Delay1→2 (page 84) D3000-97012.pdf
I meas with:
Automatic Measurements - Time Measurement Menu 3 - Delay1→2 (page 84) D3000-97012.pdf
on the DSO3000 series of scopes. Sorry.