Hi,
I'm trying to retrieve the image on my MSO6912A using the following command:
The problem is that the process never reaches an end. If i look at the display of the oscilloscope, I can see a blue progress bar stopped at around 75%, and a text saying "Remote operation in progress. Please wait".
I can only interrupt it if I send another query (*IDN? for instance). Then I receive the image, but it's incomplete and mixed with the result of the interrupting query. Something like this:
Any idea why this is happening, or what am i doing wrong?
Thanks,
Vlad Socaciu
I'm trying to retrieve the image on my MSO6912A using the following command:
The problem is that the process never reaches an end. If i look at the display of the oscilloscope, I can see a blue progress bar stopped at around 75%, and a text saying "Remote operation in progress. Please wait".
I can only interrupt it if I send another query (*IDN? for instance). Then I receive the image, but it's incomplete and mixed with the result of the interrupting query. Something like this:
Any idea why this is happening, or what am i doing wrong?
Thanks,
Vlad Socaciu
out by now hte return format is a BINBLOCK which must be parsed
by a BINBLOCK parser.