AnsweredAssumed Answered

Pass-through problem

Question asked by elmiguelestaaqui on May 7, 2009
Latest reply on May 8, 2009 by elmiguelestaaqui
Hi folks,

I'm having a problem with the PNA N5230A. I'm trying to connect to another device with the GPIB controller, because this PNA
has two GPIB ports (controller and talker/listener), with the RDEV comm to activate pass-through.
In the configuration, the GPIB port is configurated like Master Controller, with the address 21. I tried different configurations
but nothing worked.
The agilent IO suite version installed in the PNA is 14.2.
The device what I'm trying to communicate has the GPIB address 19, and I send the next command:
SYST:COMM:GPIB:RDEV:OPEN 0,19,300
but the PNA writes the next error:
+1073,"ERROR:;Problem accessing VISA library"$

What's the problem?

Thanks in advance  

Outcomes