AnsweredAssumed Answered

Read data from HP3585A with 82357B

Question asked by lucvanlangenhove on Mar 16, 2010
I used Agilent 82357B and Connection Expert to send HPIB commands to a spectrum analyzer HP3585A to retreive the data and
consequently process them via MSExcel.
In the interactive IO :
wrt"3585","D3,T4"

Following message was returned :

! VI_ERROR_TMO: A timeout occurred
Visa ErrorCode: 0xBFFF0015 (-1073807339)

Was is the corrcect way to read data (1001 values) from this spectrum analyzer ?  

Outcomes