AnsweredAssumed Answered

Enquiry On Labview Driver for PNA-L

Question asked by stanleysg on Mar 7, 2010
Latest reply on Mar 8, 2010 by bhokkan
Hi all,

i would appreciate alot if someone can answer this enquiry,

As we are usually using the PNA or PNA-X labview driver for the N5230A PNA-L, and i have downloaded from below link:

http://na.tm.agilent.com/pna/programming/

but some erros appear after using this driver, taking example of "the library 'SParametersExample.llb'.

When we run SParameters.vi, it always says "Undefined Head"" The error message is captured in jpg format.

I wonder it is normal to see such kind of error?

thanks if someone can help.  

Attachments

Outcomes