AnsweredAssumed Answered

Changing/defining trace colors in N5230A

Question asked by mart23 on Sep 2, 2008
Latest reply on Sep 5, 2008 by jvall
Hi!
Is there any method of changing/defining trace colors in N5230A? It's a 4 ports, 20GHz configuration. My company is using it for high speed Sdd21 and Scd21 measurements. We're plotting 8 traces together to check for gaps or spikes between them. After printing all the graphs it's hard to distinguish the traces apart. Some colors are almost identical. We're using one of the newest HP printers with the analyzer so the quality of the print is really good. Any help would be greatly appreciated.
Thanks. 

Outcomes