AnsweredAssumed Answered

Transfer file from PC to ENA5071B

Question asked by conchiupct on May 27, 2010
Latest reply on Jun 3, 2010 by odanzy
Hello everybody!

I'd like to transfer a TXT file from the PC to the ENA5071B. They are connected by LAN. I'm using VB6.
I'm using the :MMEMory:TRANsfer <string>,<block> command but I'm not quite sure what <block> means. I've seen this link
http://ena.tm.agilent.com/e5061b/manual ... _files.htm

But I am not quite sure... Why use "%#"? Do I have to indicate the number of bites that follows? Does the numbers of bytes should be a byte variable? Why use "b"?

Could you help me please?

Thank you very much in advance!  

Outcomes