AnsweredAssumed Answered

Using Intuilink calls in a C application

Question asked by jwagner on Jan 21, 2009
Latest reply on Jan 21, 2009 by odanzy
Hello,

I am trying to utilize the power of the Intuilink software to perform an operation that I need to do in my program. I want to capture the data in an excel spreadsheet which Intuilink does. My issue is that I cannot get the connection established to the network analyzer to be able to download the data. I have an established connection to read the marker values that I use to make my filter adjustments but when it comes time to output the data to excel it says there is no connection. How do I establish the connection to utilize Intuilink?

If this is not possible, what commands do I send to get the S11 and S21 data from the screen with both frequency and magnitude.

Thanks!!  

Outcomes