AnsweredAssumed Answered

averaging in pulse mode, external trigger

Question asked by myonezaki on Oct 12, 2010
Latest reply on May 1, 2012 by Dr_joel
pnax, using external trigger, trigger channel and point, wideband measurements, etc...trying to program the commands, of restarting averaging, using sweep averaging, setting the averages, the number of groups (if necessary) and waiting for all of this to complete before saving the data.  if there are 201 frequency points, averaging is set to 10, triggering is in point (not channel or sweep), should the analyzer be triggered 2010 times?  in the help file, manual trigger is referenced but this is not the same as external triggering?  tried using 'chan.NumberOfGroups num, sync', "with num
(long integer) Number of trigger signals the channel will receive. Choose any number between 1 and 2 million.-help file", should the num=2010?  this seemed like an infinite loop since the sweep never did complete, also the averaging notation on the screen was not shown so i know something is not right in the code.  please send an example  

Outcomes