AnsweredAssumed Answered

Unable to Return String using IVI drivers on N5230C over LAN

Question asked by mhreider on Oct 19, 2010
Latest reply on Oct 25, 2010 by odanzy
I've currently been fighting with this all afternoon. The IO monitor clearly shows the string the VNA is attempting to return, but it subsequently times out. I've fought with 2 other VNAs similarly, and only been successful using iviobj.ReadString() on the N5245A. The N5230C and two N5230As not so much. Reading Binary works perfectly fine as well on all VNAs as well as writing commands.

Note: This only occurs over LAN, using GPIB via USB all goes well. The Console on the VNA shows it is attempting to return the query as well as the Agilent IO Monitor. I've been unable to find any information on this as well.  

Outcomes