AnsweredAssumed Answered

System Verification 8719ES

Question asked by Superbrew on Oct 17, 2010
Latest reply on Nov 1, 2010 by Superbrew
I am trying to write a routine to automate the system verification. With the Sys Ver Init (Test 26) I can wait for ESB? to return 2, but this doesn't seem to work for the verification device tests. I have also tried just waiting for a long enough delay to use the KEY 60 command to simulate the Continue button press, but this is slow and unreliable. I can't see anywhere in the status byte that indicates that this routine is finished and if it passed or failed. What commands/setup would I need to use to get this done?

Thanks  

Outcomes