AnsweredAssumed Answered

SCPI Command Required for closing the session

Question asked by abhishekagarwal1982 on Oct 15, 2010
Latest reply on Oct 15, 2010 by daras
Whenever we access any module via SCPI, things are working fine. But after we are done with this somebody else wants to access this with GUI application then we are not getting full access, the module tells them that they can only change parameters as it is still in SCPI Remote mode. The workaround we have found is to access it the unit with remote desktop, shut down the module, restart and then it is ready to be accessed. Isn’t there a command that is closing the SCPI session??  

Outcomes