AnsweredAssumed Answered

Unable to close an Opened session in TCL

Question asked by kelly on Sep 1, 2010
Latest reply on Sep 1, 2010 by odanzy
Hi all,
I have a set of automated tests which are in TCL which basically performs a repetitve tasks over LAN for a very long time. The next time when i start the same test , it's not able to connect to the IP address. I beleive the session which had been opened during the previous run isn't closing resulting in connection failure.

Now since the whole script is in TCL , i am unable to map it to the built in (Close() ) function of the Agilent library. How can i close the session in TCl . I am using the GlobalMgr.dll as the COM file which doesn't seem to have a Close() function. Please have a look at the screenshot.

Thanks
Kelly  

Attachments

Outcomes