AnsweredAssumed Answered

HP 3577B connection with LabView

Question asked by dankotom on Aug 19, 2010
Latest reply on Oct 24, 2012 by sponte
I tried to connect my HP3577B via expresscard GPIB to LabView 2009. "Scan for instruments" in LabView gives an error. i have 3 questions:

1) How can I set GPIB address on HP3577B?
2) 3577b doesn't recognize the *IDN? query from LabView. What should I do?
3) Anybody has 3577B operational manual? I have it for 3577A but setting the GPIB address as it is explained doesn't work for 3577B  

Outcomes