AnsweredAssumed Answered

HP8719c remote communications using Vee pro 9.2

Question asked by jsjlaval on Aug 4, 2010
Latest reply on Aug 5, 2010 by Dr_joel
Hello,

I have a problem using Panel Driver (Vee) on Live from HP8719 Network Analyzer.
In fact, I want to retrieve the output values from Analyzer via PC.
So, I added a output data "Active_CH_Trace1" on Panel Driver and I connected this output to Graphe XY.
And I reatrieve the values after clicking to "Run" but the problem is when I try to change the measurement of another parameters (S21,S22...) from Panel Driver,
I have a "VEE Run Time error" and I do not have anymore the control of analyzer.
How can I keep the control of Network Analyzer even after running the programme?
Thank you.  

Outcomes