AnsweredAssumed Answered

Format Data for complex readout

Question asked by ronrodrig57 on May 21, 2009
Latest reply on May 21, 2009 by ronrodrig57
Hello, I have an E8361A. I'm trying to read real/imag data, using labview. When I use the format display :CALC1:FORM MLOG.. I get an error. If I comment out that statement, then my :FORM:DATA ASC;:CALC1:DATA? SDATA... doesn't work(or FDATA)- it hangs and I have to exit labview. This occurs regardless of saving the state/cal file in Mag Log or Mag Lin and/or setting the display format in Mag Log or Mag Lin. Other info: I'm recalling that S22 state/cal file and doing the usual settings for mech standards, 56.8GHz to 57.02GHz  

Outcomes