AnsweredAssumed Answered

Using PNA-X port 2 connected to ECal port A

Question asked by miyamky on Aug 2, 2010
Latest reply on Aug 10, 2010 by miyamky
I'm programming a calibration.  The cals done w/ the ECal module connected at port A to the PNA-X port 1 work fine.  So now I'm trying to do a calibration w/ the ECal module connected at port A but now the PNA-X port 2.  If I do a cal through the Cal Wizard, I can specify port 2 for the calibration and all is well.  However, I'm unable to find the SCPI commands to tell the PNA-X to use port 2 (instead of port 1) for the ECal calibration.  Please advise.  

Outcomes