AnsweredAssumed Answered

FOM in Segment Sweep

Question asked by antennas4space on Apr 26, 2010
Latest reply on Apr 26, 2010 by daras
I see that the FOM now allows primary frequencies > the PNA-X maximum frequency. That is, I can specify that we have a tripler (source divisor=3), such that the Primary frequency is 90 GHz, but the source is 30 GHz. That works fine with a normal start/stop linear sweep. Either a manual setup or using mmWave macro works fine.

However, in Segment Sweep mode, the dialog boxes limit the frequency to the PNA-X maximum source frequency.

Can the firmware be modified to allow the same capability as with the normal linear sweep?

I think the CW Time sweep is also similarly limited.

Regards, and thanks!  

Outcomes