AnsweredAssumed Answered

Power sweep measurement

Question asked by Hidayah on Mar 26, 2008
Latest reply on Apr 5, 2008 by Hidayah
Hi,

Could some tell me where are wrong with my transactions that I write in the file attached here. I write and modify the transactions based on the example that I found from PNA help. But got error.

I did manually the setting in the PNA to get the measurement that I want. Then I write the transactions based on the setting.

First I will need to select channel 1. Then select the sweep type for power sweep setting. The start power and stop power for this power sweep setting is -10 dBm. The CW frequency is 2.45 GHz. Then I need to select channel 2 for S21 measurement. Same as channel 1 setting, first I will need to select channel 2. Then select the sweep type for power sweep setting. The start power and stop power for this power sweep setting is -10 dBm. The CW frequency is 2.45 GHz. After That I put a marker for S21 measurement on channel 2. I want to read the data from y-axis. Thanks.


Regards,
Dayah  

Attachments

Outcomes