AnsweredAssumed Answered

Can you apply external cal data to Source Power cal's

Question asked by cgantz2000 on Nov 30, 2009
Latest reply on Dec 21, 2009 by daras
Hi all.

We have fixed cables, pads, etc. attached to our DUT for which we have cal data, but it can't be included in the source power cal.

Is there a way to apply our cal data to the PNA-X source power cal data so that we have known powers delivered to the DUT. There is a function  getSourcePowerCalDataEx, plus the corresponding set function, that sound like it should allow us to apply our corrections, but it doesn't seem to deliver the data that I expect.  getSourcePowerCalDataEx  just gives me an array with the same value in each array element.

Also, unrelated to the above, the GetXAxisValues2 doesn't seem to match the documentation, and when I try to use it, the program gets stuck in the function. The documentation says that parameter 2, data, should be an array of double. But in the program it only takes a double. I'm using C#, and PNA-X version 9. The  GetXAxisValues function works fine.

Chuck  

Outcomes