AnsweredAssumed Answered

Is it the setting error (PNA E8362B) ?

Question asked by Hidayah on Mar 12, 2008
Latest reply on Mar 12, 2008 by odanzy
Hi,

From the previous discussion about my PNA E8362B, I tried to only write transaction EXECUTE CLEAR in the my PNA-L direct IO but also got error. Is it this is because of setting problem ? I change the PNA-L to live mode. But still got error. If I run the block with NOT LIVE mode, then will be no error. Could someone tell me what is the problem with my VEE file ?
Thanks.

Regards,
Dayah  

Outcomes