AnsweredAssumed Answered

Print To File object method on a PNA

Question asked by jamesh on Jan 23, 2011
Latest reply on Jan 23, 2011 by jamesh
Hi,
PNA 5230C
Firmware revision: A.09.22.15

The print to file method under the app object does not print a file to a remote computer path. For example Path :"\\ws211\c$\test.jpg". There is no error returned from the PNA. However using the PNA front panel File menu Print sub menu "Print to file" works perfectly with the same path entered into the "save as" dialogue window.

If the printToFile method only allows local file saving, is there an object method for moving the local file to a remote location ?

Thanks in advance.
Regards
James  

Outcomes