AnsweredAssumed Answered

need help: Agilent E4980A LCR meter through GPIB. Labview

Question asked by cxcissy on Jan 30, 2008
Latest reply on Feb 10, 2008 by odanzy
Dear Sir/Madam,

I am new to Labview and now trying to communicate with Agilent E4980A through GPIB. First, I try to set up all the parameters in the front panel. I can set the frequency sending strings "FREQ 1000 (for instance)" to data input of GPIB write VI. But I cannot set other parameters in that way. I am wondering if there should be some commands to comunicate with E4980A, but I cannot find them. There are commands in the manual, but it looks like C language or so, I don't know if I can use the commands and how to use them in Labview. So I really need help, Thank you very much!!  

Outcomes