AnsweredAssumed Answered

From 8753D to N5230A, programming questions

Question asked by manuamador on Jun 17, 2008
Latest reply on Jun 18, 2008 by manuamador
Hello,

I am working on a 8753D Network analyzer. The network analyzer is driven  by a PC with a Labwindows/CVI 5.5 program and a motor is driven by the same program. Our setup is upgraded with a N5230A  PNA. I am wondering if  I'll have to start form scratch or if I can use the same program with minor adjustements.

I have heard of DCOM, I believe it is a driver-free method, but I am not really into starting a program from scratch.  

Outcomes