AnsweredAssumed Answered

Any DCOM programming examples for GCA on PNA-X?

Question asked by dhfx on May 8, 2009
Latest reply on May 11, 2009 by dhfx
Are there any programming examples using DCOM for setting up and performing a GCA measurement sweep on a PNA-X? The macro example in the online help uses SCPI commands via the parser instead of real DCOM method calls, and (I may be mistaken but) I don't see any code there for actually running the measurement on a DUT.

Also, can GCA be run as a wideband pulse measurement using external trigger (Meas Trig In) to acquire the data in the middle of the pulse?

David Friedman
Sr. Principal Engr.
Symtx, Inc.
Austin, TX  

Outcomes