AnsweredAssumed Answered

The Problem of controling N5242 by GPIB

Question asked by xqzhao on Sep 7, 2009
Latest reply on Sep 8, 2009 by Dr_joel
In my application,when i use GPIB to control N5242,I meet many problems.
one:In my Application the default filter type can not meet my needs,So i want to change the filter type to determine whether other filter type is the wanted.When i set the stage3's filter type with PWIN,I have to setting the Parameters:"P","D","W" and "R",but i do not the meaning of them,so i can not use this filter type.
two:In my Application,I want to use the 120K IF Bandwidth,so i calculate the two stages's COEF uing Matlab,But when i input the COEF into it by GPIB,I can not get the correct result,sometime can not scan.I do not know the reason.
Any help is appreciated!THANKS!  

Outcomes