AnsweredAssumed Answered

Return VNA to local state

Question asked by scroteau on Aug 19, 2009
Latest reply on Aug 19, 2009 by odanzy
Hi all,

Setup
Visual Basic 2005
Agilent IO Libraries Suite 15.1
VNA 8714C
Agilent 82357B USB/GPIB Interface

using

Ivi.Visa.Interop.ResourceManager
Ivi.Visa.Interop.FormattedIO488

to access device which works just fine. The problem I am having is I can not figure out how to toggle the REN line to put the device back in local mode?

I have found then Ivi.Visa.Interop.IGpib interface but I can not figure out how to open/access the interface and use its method ControlREN?

Thanks in advance for the help.
Scott  

Outcomes