AnsweredAssumed Answered

PNA-X VXI-11 Connection

Question asked by andyTPE on Aug 16, 2011
Latest reply on Aug 17, 2011 by bhokkan
Hello Component Test Division,

I just received an N5242A-H85 that shipped with A.09.33.09 firmware.  Previously I have been automating this model of VNA using the 5025 socket port.  However, I discovered that this instrument/firmware release now supports the VXI-11 stack (at least according to Agilent IO Libs).  Please can you confirm - I could not see anything in the help file on this being a new feature...

Does this mean that you support SRQ's via LAN?

Thanks and keep up the good work....

Andy  

Outcomes