AnsweredAssumed Answered

Help on HP54601A firmware ...

Question asked by stewart_lee on Jun 11, 2007
Latest reply on Jun 12, 2007 by stewart_lee
Hi, you scope experts,

I use a 54601a for everyday debug work, it's a pretty good piece of instrument. But the display mode only available in dots mode, can't show a vector trace like the 54602B does, it connects the dots forming a continuous trace. That's useful especially for looking for abnormal pulses.

So, is it possible to upgrade the firmware to obtain the "connecting dots" display mode? Or, can I use a copy of the 54602B ROM on the 54601A? Since both of them are 4 channels and 20MSPS.

Hopefully I can get answers here, also I hope to meet some designers of this great scope here.

Best regards
Stewart  

Outcomes