For example, features like min/max/average would be very helpful on buses or frequency measurement on single bits.
There are plenty of occasions where I'd personally find this useful, particularly in debugging DSP designs where you have test data being output digitally from an FPGA or similar.
Unfortunately the series 8000 do not have such features, however I can suggest it for an enhancement. Thanks for the clarification on how these features will be useful for the digital channels.
There are plenty of occasions where I'd personally find this useful, particularly in debugging DSP designs where you have test data being output digitally from an FPGA or similar.
Thanks,
Jon