AnsweredAssumed Answered

Saving more than 1000 Data Points.

Question asked by ElCapitan on Apr 21, 2007
Latest reply on Apr 24, 2007 by dnt
Hi
I can’t save more than 1000 data points with a 6014A scope.  The acquisition is stopped and the scope is in normal mode.

Regarding to the Manual it should be possible to increase the length but I don’t work for me:

[…]Length sets the number of data points that will be output to the file. Length can be set to 100, 250, 500, or 1000 when the acquisition is running or more when the acquisition is stopped. […]

http://cp.literature.agilent.com/litweb ... -97011.pdf  page 247

Updating the scope firmware doesn’t help.

Have someone a solution for this Problem?  

Outcomes