When multiple digital buses are enabled, the digital bus decode window only seems to display entries when the value of a bus changes, rather than when the buses state clock has an edge.
E.g. if a bus has the value of 0x8 for eight cycles, there will only be one row in the decode table and one entry when you save the data.
Is there a way to change this?
Although I can see the current mode being useful in some applications, it is not helpful in lots of others, especially as there appears to be no other way to save the bus waveform.
Thanks,
Jon
E.g. if a bus has the value of 0x8 for eight cycles, there will only be one row in the decode table and one entry when you save the data.
Is there a way to change this?
Although I can see the current mode being useful in some applications, it is not helpful in lots of others, especially as there appears to be no other way to save the bus waveform.
Thanks,
Jon
Attachments
I do file/save/waveform..
Set type: .csv
Source: Bus 1
On-screen data: True
And I get this - which doesn't correlate to what I see on screen (see attachment).
-1.26E-03 0xD
-1.26E-03 0xB
-1.26E-03 0xD
-1.26E-03 0xD
-1.26E-03 0xE
-1.26E-03 0xD
-1.26E-03 0xA
Attachments