AnsweredAssumed Answered

Calibration

Question asked by KirkSummers on Feb 16, 2011
Latest reply on Feb 17, 2011 by odanzy
I recently sent in a E5071C ENA Network Analyzer for calibration. To give a bit of background information, this equipment has a removable hard drive because I am working with classified data. When I sent it in for calibration, I sent an unclassified drive with the equipment and now I need to transfer the calibration information to the classified drive that I use everyday in the equipment. Can you tell me what type of file(s) the calibration data is stored to and where the file(s) is/are located on the drives so I can copy them over to the classified drives? Or is the calibration information for this equipment stored in the system memory? Thanks!  

Outcomes