AnsweredAssumed Answered

85060C Ecal and 8753D

Question asked by MICROWAVE68 on Sep 12, 2008
Latest reply on Sep 15, 2008 by MICROWAVE68
I have a 8753D as well as a 85060C and 85093A however it didnt seem to work, i dont have a manual for the 85060 so im kinda lost, i hooked up the GPIB from the 85060 to the 8753 and set the adress switches on the back of the 85060 to match the VNA adress, when i power both units up the 85060 goes through its selftest sequence but when i push the button the green LED blinks but nothing happens on the 8753D.
It is my understanding that the 85060 is supposed to control the 8753D or am i wrong here ?  

Outcomes