AnsweredAssumed Answered

Measurement Result cannot display on the screen

Question asked by fion on Nov 15, 2006
Latest reply on Nov 16, 2006 by odanzy
Hi, all.

I am used Agilent VEE Pro to write the program. I Need some information regarding DSO3102A Oscilloscope. The problem faced by me is the measurement  result cannot display on the screen. For example, VPP, PERIod....

I issued command like what stated in the Programmer's reference, for example:

":MEASure:VPP:CHANnel1". This command displays the on-screen peak-to-peak voltage measurement. But, the measurement result still cannot display on the screen.

When i used the front panel to measure the VPP. The VPP result will display in the left-bottom side. Is it remote command also can have the same result? Or do i need to specify something on command or i need to do issue some initialise commands at the beginning of the program? Anyone can help me on this.
Thanks.  

Outcomes