AnsweredAssumed Answered

PNA unguided calibration standards

Question asked by yarien on Jul 14, 2006
Latest reply on Jul 14, 2006 by yarien
I am performing a Unguided TRL calibration in x-band with COM in HPVee.
For this I have to measure: Thru, Line and Reflect (on port 1 and 2)
With the command
"Calibrator.AcquireCalStandard2(naTRL_Reflection,1,naNotSlidingStd);"
I can ask the analyzer to perform the reflection standard on the Port 1.

How do I ask the analyzer to perform the measurement on Port2??

Is there a way to sees which calibration steps the analyzer has performed after calibration?

Lots of thanks

Yoeri  

Outcomes