AnsweredAssumed Answered

Using COM to switch to millimeter wave config

Question asked by pnaCOMuser on Aug 14, 2006
Latest reply on Aug 14, 2006 by Dr_joel
We have an 8363B PNA with a N5260A millimeter wave controller and some OML heads connected to it.  It's a banded configuration, so we can't do a single sweep from the low frequency all the way up to millimeter waves (no need to).

Just the same, I'm wondering if it's possible using COM objects to remotely switch from the typical test test to the millimeter wave setup.  The "ExternalTestsets" collection looks promising, but there's no mention of N5260A in that end of the help file.

Thanks!  

Outcomes